Hi,
We've developed a 4S6P pack with the BQ40Z60.
Discharge stops at 2750mV / delay 5sec, based upon CUV
To preserve capacity after full discharge, we've set Power - Shutdown voltage @ 2750mV / delay 10sec
For charging we've set:
Pre-charge start voltage 2200mV
Charging voltage low 2900mV
Precharging current 250mA
Charging current low 1000mA
If the battery is left alone for a while after full discharge, the battery goes into shutdown. Leaving for a longer period will drop the voltage further.
The problem we've got is the BMS wakes up when a charger is connected but does not start charging at all.