This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM61460EVM: Schematic for a 6V Output

Part Number: LM61460EVM


Hi.

I am using the same schematic as the Evaluation Board with the EMI Filter to output 6V and 6A, I just changed RFBB (R20 on my schematic) to 20K to get to 6V. This schematic with be on a PCB with an MSP432 as well as a GPS receiver. The Load will range from 1A to 6A depending on the amount of devices connected to the board. Is there any additional re-tunnig I need to do for the oscillation loop or anything else to accommodate for the different load currents.