Ulrich
We removed the controller- and measured NTC pin to be 3 7.4 Ohms.
Any idea on the ways this can happen:
1- ESD?
Then only on 1 pin?
2- somehow external circuitry applied higher than 7V?...kind of out of real possibility...there is no such circuitry in proximity.
3- Our choice of a resistor is not correct- one should use NTC?
We can find NTC right here where are doing all this work.. ...of old-style in penny size disk! Cannot get SMD before next week...
Any help/review/comment will be so helpful again.
robin