This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5143-Q1: Two input single output Operation

Part Number: LM5143-Q1


Hi,


I would like to use one LM5143-Q1 to parallelize 2 battery packs and produce 12V at the output. For this, the input of each phase, the drain of the upper FET would be connected to a different battery pack. I would like to know what happened in the case that 1 battery packs fail, and I disable one of the two phases of the converter. Thanks

Pablo Oliva