I have put together a design based on the webench power designer that allows for 9v to 60V input 50V output up to 0.5A.
I'm not an expert at laying out the circuit and between the person that laid out the board with this part on and myself reviewing we feel we could use another set of eyes to make sure there are no real glaring errors.
As well just a quick glance at the BOM would be appreciated. Could I upload these 2 files for any feedback from TI?
(CK plot and BOM)
Regards,
Brad Mitchell