This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61500: Does this drive support the configuration in parallel "8s8p"?

Part Number: TPS61500
Other Parts Discussed in Thread: LP8555, TPS61196

Hi,

I`ve an application that requires drive up to 64 LEDs in constant current mode. I going to use a 12V source. The LED has the following parameters:

Foward voltage: 3.2V

Foward current: 150mA

Is TPS61500 suitable for the desing 8s8p?