Other Parts Discussed in Thread: LM5576,
Hi,
can LM5575 and LM5576 devices be synchronized via their pin SYNC ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
Yes, it can, below is Sync pin description
The internal oscillator can be synchronized to an external clock with an external pull-down device. Multiple LM5576 devices can be synchronized together by connection of their SYNC pins.
Hi, thanks for the reply,
so I suppose that an lm5575 device can synchronize an lm5576 and vice versa. It's true?
Hi
Yes, you can use external clock to connect syn pin of LM5575 and LM5576 . let them working at same fsw.
Thanks
Daniel Li