This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54360: EMI issue on 80MHz

Part Number: TPS54360


Team,

Would you give me some suggestion for 80MHz EMI issue?

Regards,

Roy

  • Hello Roy,

    Design is using a tremendously large inductor.

    With big inductor comes big EMI problems.

    I would confirm that common mode choke has high impedance in that frequency range.

    Additionally, you are lacking input capacitor close to the IC pin (pin 2) of the device.

    A small value, say 220nF, should be placed close to IC pin. ground connection should have low impedance between PGND.