Other Parts Discussed in Thread: BQ51013B,
Hi,
We are designing a medical wearable that will use wireless charging. Due to size constraints, your BQ51050B Wireless Power Receiver and Battery Charger appears to be the perfect choice for this design since it is a one chip solution. I have acquired your BQ51050BEVM and have run preliminary breadboard testing and it appears to work well. I have just started to look at FOD calibration and have run into some issues. I downloaded your FODCalibration.exe program and installed it on my computer. To test it before taking my own data, I tried to run it with the supplied “Real Calibration Example.txt” file. As instructed, I set the Part # to BQ51013B and loaded the example file and pressed Next. On the Vos Calibration page, I was able to get a reasonable model graph by changing the Vos field, but on the next page, RFOD/Ros Tuning, the program was completely unresponsive to changes in the Ros value. If upon entering the page I first adjusted the RFOD value, the graph was responsive. But after I attempted to make any change to the Ros value, the graph was no longer responsive, even if I then went back and changed the RFOD value.
To see if this was a Windows 10 issue, I then installed the program onto a Windows 7 machine, but the behavior was identical. Do you know why this is not working?
If the program doesn’t work, I could try to calculate the values manually. Since your documentation gives no information at all about calculating the Rfod and Ros resistors, can you provide any help in the way of equations and a more detailed description of the FOD/resistor divider operation so I can manually calculate and adjust the values based on obtained data?
Also, we don't need Qi qualification on this product but it would be good if it worked with most Qi chargers. So if there was a way to "maximize" the FOD tolerance so it wouldn't "get in the way" of a successful charging session, that would be useful. Again, from a design standpoint, it would be good to have some documentation that explained the FOD operation in the BQ51050B and the setting resistors calculation requirements.
Thanks,
Glenn