This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir/Madam,
My customer is asking to review TPS62410 schematic. Could you please review the attached schematic?
Vin ; 4.4V
Convertor #1 (MAIN_3.3V) output ; 3.3V / continuous current load 0.6A
Convertor #2 (RFID_VCC) output ; 3.3V / continuous current load 0.6A
Regards,
YY.
Hi Kim,
I reviewed the schematic and could not spot any problem.
Please note that the device is optimized to operate with inductors of 2.2 μH to 4.7 μH and output capacitors of 10 μF to 22 μF. Beyond the datasheet recommendations, it is the customer's responsibility to ensure loop stability.
Please also make sure that EN pin voltage is always stable for the proper functioning of the device.
Regards,
Febin