This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z80: bq40z80 EMSHUT exit

Expert 1205 points
Part Number: BQ40Z80

Hello,

I'm entering Emergency Shutdown by setting SHUTDN low (0V).

Then i want to exit by:

Voltage at Pack pin > Charger Present Threshold for two sample periods (that is, ~500 ms). This exit condition requires the [EMSHUT_EXIT_VPACK] bit to be set.

I had also Power->Power Off->Timeout parameter sert to 1 (could',t it be less than 1min?)

And nothing happen - I can't exit EMSHUT mode applying VBAT to PACK even more than 5 seconds.

Am I missing something?

Maybe I can share my *.gg file?

Regards,

Adam