Hi,
I am using 1S6P combination in Li-ion Battery pack.
I have build charger using BQ24600. I set a charge current to 3A. When battery pack is at 2.7V , and i am trying to recharge the battery. Charger charging battery at pre-charge current (300 mA). it continues upto 30 minutes. in my case due to these 1S6P combination, Battery pack doesn't reach at 3.3v within 30 minutes and timer expires and Charging is stopped. To reset these condition i need to either toggle CE pin or POR. Is there any other way to apart from above to reset 30 minute timer? What is the minimum low pulse is required to toggle CE pin?
While fast charging at room temperature, the battery pack temperature rises above 45 degree and charging stopped. Is there any other way so that temperature doesn't rise beyond 45 degree.?