When tps54331 is short circuited to the ground, the temperature of the chip will rise, which will cause the chip to fail due to the over temperature of the device caused by the junction temperature. What measures can be taken to reduce the current and temperature during chip short circuit.