Other Parts Discussed in Thread: REF3133, REF3333
Hi,
My customers use REF3030 (SOT-23-3) to power the MCU (input 3.3V, output 3V):
During the ESD air (6KV) test, when powering the MCU, 3V will drop, causing the power to restart.
They also moved the two CAP C3011, C3000 close to the IC, but not any improved.
If REF3030 is replaced with 431 the ESD test can be pass 20KV and meet the requirements;
Is there any TI can provide help or reference design, or can I find a better ESD Voltage Reference IC?
Regards
Rock