Part Number: BQ25703A
Hello team,
There are an unexpected behavior at the BQ25703A, and three questions.
・Behavior
When writing 0 from 1 at ChargeOption3 Register (I2C address = 35h) bit7: EN_HIZ, InputVoltage Register (I2C address = 0B/0Ah will be changed from set value.
This is checked by both reading resister and actual.
・Questions
1, Is this behavior expected?
2, I recognized that InputVoltage register is written when CHRG_OK pin is changed to H from L, but in above situation CHRG_OK pin is still not changed. Do you know other trigger to pull it up?
3, Is there any way to prevent to change InputVoltage register?
Regards,
Hideki