Other Parts Discussed in Thread: TPS650330-Q1
Hi team,
My customer requires PMIC for below power supply requirement.
- Vin = 5V+/- 0.2V
- 1.2V : 310mA max
- 1.8V: 227mA max
- 2.8V: 40mA max
- Ta= 95degC
Is there any concern to apply TPS65000-Q1 with below cnfiguration?
- VINDCDC = 5V, VDCDC=1.2V
- VINLDO1 = 5V, VLDO1=1.8V
- VINLDO2 = 5V, VLDO2 = 2.8V
From Power dissipation point of view, I expect 0.904W.
Best regards