This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC21732-Q1: the function of Hybrid pull-up structure

Part Number: UCC21732-Q1


Dear team,

The datasheet said that this structure is to achieve rail to rail output. Can't a single NMOS or PMOS achieve rail to rail output? At the first, the NMOS takes in charge until the output increase to VDD-3, then the PMOS takes in charge. Why NMOS don't continue to take in charge when output>VDD-3?

Thanks & Best Regards,

Sherry

  • Hi Sherry,

    Welcome to E2E!

    The initial stage, when both NMOS and PMOS are active, allows to drive a higher current. Once the output reaches VDD-3V the NMOS will shutdown because it needs a VGS>3V (threshold voltage) to operate.

    Best regards,

    Andy Robles