This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62088: Use as Power/GND (source/sink) switch?

Part Number: TPS62088

HI,

Is it possible to use the TPS62088 as a  Source or  Sink switch?   So Either Source (Vout = Vin)  or Sink current (Vout = GND).   I see in the datasheet that 100% duty cycle operation is supported (Vout =Vin)  which I think covers the Source part,   Is 0% duty cycle supported to allow this component to operate as a current sink?

If it's possible would there be any restrictions beyond what is in the datasheet?  I expect Max current to be ~ 2Amps .

Thanks,

Roy