Other Parts Discussed in Thread: CSD17581Q5A
Hi,
my customer has been using CSD19505KCS for long and now they find some devices break down during the test. They suspect that using different LTC CSD19505 in parallel may be the cause of the break down, since the parameter mismatch may cause some MOSFETs to turn on before others, which exceeds the maximum rating of the device.
I would like to know:
1. Is it true that we should not use different LTC CSD19505KCS in parallel?
2. What considerations need to be taken when connecting MOSFETs in parallel?
3. If we connect 5 MOSFETs in parallel, and the peak current needed is 100A, what current rating MOSFETs do we need?