Ulrich:
3rd proto got stuck with SWS pin at 2V. 121 Ohms ( R22 in Eval kit) shows 12.5 mA current. HVG stuck at like .4V.
We have tried reflow of new controllers suspecting pad cold solder. Did nothing.
We spent a day dead bug fashion hookup of the controller to make sure all pins get connected.
Exact the same observation.
Do these results tell us anything about the underlying issue?
i.e
- Depletion source is stuck at 2v
- HVG at .4 v
- R22 carries 12.5 mA
We have found no errors in the 3rd proto. Yet, on first power-up, it worked exactly as expected. We then hooked up the xmfr. & so far, never got it back to work.
Yet we are trying to follow the Debugging Startup failures Document as well as we can.
Other two protos we had to abandon due to some damage from repeated rework. But as you recall, we had the start-up working. There was no PWML so our idea was to go to 3rd proto in order to eliminate chances of open circuits .
Any insight will be immensely helpful as we are dead against a serious situation.
robin