This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/BQ78412: SOC jumps at high and low temperatures

Part Number: BQ78412
Other Parts Discussed in Thread: GPCCHEM

Tool/software: Code Composer Studio

Dear,

I contacted the Customer support center and they advised me to post my question to this form.

The problem I'm encountering is that the SOC jumps suddenly from 68% to 0% SOC for low temperatures and during charging at high temperature (50°C) jumps from 0% to 30% . I tested with different bq78412 chips and see the same behaviour at high (+50°C) and low temperatures (-15°C). The SOC curve is linear for temperatures between the 15-25°C so I see the strange behaviour only at extreme low/high temperatures. How can I resolve this problem