Hello,
I have a TPS2511 circuit that is intended to charge newer Samsung Tab A Tablet (T510 Series) but the charge current never goes about 100mA. Is there something that is wrong with the circuit or is the Tab A so new that it doesn't recognize any of the legacy handshaking protocols?
I'll attach a screenshot of the schematic and a waveform showing the D+ and D- signals when the cable is plugged in. The current limit resistor is set to 44.2K so it should be able to supply 1.2A.