Hi.
I am trying to make a PWM generator with UCC35705.The design tool of TI is used to calculate the frequency and duty cycle.
The working mode is selected in Mode 1.At present, I have connected a set of 10uF/50V electrolytic capacitors and 104 non-polar capacitors in parallel between VDD and GND.
The chip can successfully generate PWM waves and the duty cycle and frequency are the same as my calculation results.
However, after nearly 5 seconds of power on, the capacitor starts to generate a lot of heat, and the PWM disappears and the chip stops working.
Please help me check whether my design is correct. Can this chip be made into an open-loop system as my design?
Attached is the schematic diagram.
thank you.
Echo Wang0243.TI.pdf