Dear E2E,
within our team we are using the TPS63051 in a Li-ion battery powered application within a custom miniaturized PCB, which needs 3V3 constant output voltage for powering all the components. I followed all the design suggestions for the choice of the components associated to the regulator (see the image attached).
Although, during normal operations, the voltage is constant 3V3 but the current measured from the battery is strongly inconstant, with a mean of 23mA (which is the expected value) but a waveform with continuous oscillations between the values -20 mA to around 100 mA (one hundred) with a period of around 14us. I attached an image from the oscilloscope showing this measurement.
This behavior (oscillations) is not anymore present if we power the device downstream of the regulator, so we suspect that the issue come from there. We also observed that trying to filter the path from the battery to the device with inductors improves the current waveform (becomes more constant).
Do you have any suggestions on the possible cause of this issue and on how to solve it?
Thank you very much in advance.
Best regards,
Gianluca Milani