This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: Automatic operation of DDSG/DCHG depending on LOAD/Charger

Part Number: BQ76952
Other Parts Discussed in Thread: BQSTUDIO

Hi,

I am using DCHG and DDSG to drive low side FETs.

Are DCHG and DDSG enabled or disabled automatically according to LOAD/Charger detection at AFE end or do we need to implement it with the help of exetrnal MCU by reading data from AFE and then sending back commands to actuate DCHG/DDSG?

Another question is whether CHG/DSG also work automatically, because right now I have been testing these pins with the help of BQStudio by actuating them by commands.

Regards,

Anurag