部品番号: BQ24610
We are currently designing a charger using bq24610.
The battery used is equipped with bq40Z50 and is connected to the charger in the shutdown mode of bq40Z50.
I'm going to use 125mA charge of battery detection flow of bq24610 to release this shutdown mode.
1. 1. How long (length of time) does the 125mA charge of the battery detection flow of bq24610 start after setting the CE terminal to H? The VFB at this time is 0V (because the battery is in shutdown mode).