Other Parts Discussed in Thread: BQ24075
Hi all,
My customer considers to use BQ24070 for his end product and provided a question.
[Question]
Is it ok to apply 3~4.2V when VIN=0V?
(Does the device stay sleep mode since VIN=0V and device will not be damaged?)
[Background of this question]
When BQ24070 is operating and battery is absent, the BAT pin cycles between charge done (VO(REG)) and charging as described in 8.4.3.5 Battery Voltage Regulation.
In such a case, if STAT pin is connected to LED, LED blinks.
In order to prevent this situation, the customer attempts to connect CE pin to battery and add pull down resistor so that device can operate only in case that VIN and battery exist and the device can't operate if Vin exists and battery is absent.
Best regards,
Shota Mago