Dears
We have make the BQ34Z100-G1 in LED mode 0, and the Alert pin will be PIN1, and based table 22 to set the Alert Configuration Register Bit Definitions.
After enable the BATLOW alert function, and with a low voltage battery, the alert have 1s low and 7s high, not a continue low.
So need your help if this is right for the alert function? we think in a alert condition, the Alert must continue low?
Thanks
Jun Shen