1. Measure the temperature rise of the Top case, assuming that 40% (this is from TI reference data) power consumption is calculated by TOP heat dissipation, so calculate Rthja=Rthjc+Rthca, and then calculate Tj, the result is 173C, fail;
2. Test the Bot case (measure the temperature of the copper foil close to the Bottom case), calculate with the thermal resistance RJC, and have not tested this way yet