Hi,
I want one EVM which includes battery charging circuit for 26V battery and the input voltage range is 30~36V DC, if possible I2C programmable. Can anyone suggest the suitable board for my requirement.
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Nimtha,
The only battery charge controller that the TI battery charge group with this input and output range is for lead-acid batteries: BQ24450.
TI currently does not have a single IC LiIon charger or charge controller capable of up to 36V input and 26V output. You might find a multi-IC reference design for your application at
Regards,
Jeff
Hi Jeff,
Input I can reduce to any required voltage but I need to support the charging circuit for lithium polymer battery of 26V (25.9V). Can you suggest any design for that if possible at least the charging IC available. As of now with our current battery board we are using BQ24735RGR to support 14.8V battery. But this will not support for 25.9V battery, we need to include the higher voltage to our board.
Thanks,
Hi Namitha,
For linear charging, you can used BQ24450. If you can customize your input voltage to track the battery voltage, thereby keeping the chargers IN to OUT ration constant, this linear option could be as efficient as a switching charger.
For the switching buck converter based option, the BQ24610, capable of input up to 28V is an option.
Regards,
Jeff