Dear *
1) ON or OFF on high side [isolated gate driver]
can you propose a isolated gate driver that can drive following two mosfets ( BSC600N25NS3 [250V] and BSC12DN20NS3 [200V])
An alternative to HT0740
2) in switching applications [ low side gate driver]
can you propose a gate driver to drive low side mosfet ( BSC600N25NS3 [250V] or BSC12DN20NS3 [200V]) of buck-boost
2a) if converter working at 1MHz to 2MHz
2b) if converter working at 150kHz to 650KHz
An alternative to UCC37322D ( we are using UCC37322D at fsw = 200kHz and driving IRFB31N20DPBF mosfet)
Best Regards,
David.