This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A8300: BIAS pin

Part Number: TPS7A8300


Hi experts,

My customer have 3 circuits that use the TPS7A8300.  Each has a VIN of 1.2V, 1.4V, and 1.8V.  The BIAS to all of them were connected to 5V.  Can they leave the 5V connected to BIAS when VIN is 1.4V and 1.8V, or do they need to disconnect the 5V from the BIAS pin? 

Any disadvantages for leaving the BIAS connected to 5V?

Thanks,

Connie