This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65185: Schematic review

Part Number: TPS65185

Hi,

I have some issues with my PMIC, none of the rail are coming up when I pulled up WAKEUP and POWERUP, and I cannot access the device through I2C.

I ordered some extra chips to try to switch it, in case I overheated it, but I would like to make sure that my problems are not coming from design issues.

Can you help me reviewing my schematic (I pull up the POWERUP pin externally and Vin voltage is 3.2V).

Also, is to ok to left POWERUP floating if I use the I2C register to turn the PMIC in ACTIVE mode, or should it be pulled-up or connect to WAKEUP?

Best,

Vincent L.