This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24041: bq24041 ASI

Part Number: BQ24041


Dear team,

How to connect ASI when using external input and not use external input?

Thanks.

Best regards,

Sammi

  • Sammi,

    To connect the ASI with an external input, the pin can be connected directly. It is not required to have the ASI signal pulled high if bypassing the VIN > VBAT + VDT requirement for ASO is possible and can be left floating as it is internally pulled down. It is not possible to power the device without an external power supply without an external power source such as the IN or OUT.

    See images below