This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TPS61089: TPS61089 debug the problem

Part Number: TPS61089

Tool/software: Code Composer Studio

The battery is 3.7V/10A. TPS61089 is used to boost the voltage to 9V to supply the motor, and the motor is 6W. The voltage sag of the battery is 3.3V when the load is turned on