This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25942L: DMODE, PGOOD, and IMON-pins

Part Number: TPS25942L


Hi Team,

My customer is considering to use the TPS25942L. Could you support the following questions?

Customer doesn't use the Diode Mode, Power Good, and Current Monitoring. In this case, how should these pins be treated(e.g. open or tied to GND)?

1. DMODE-pin(Diode Mode): Open?

2. PGOOD-pin(Power Good) : open or tied to ground

3. IMON-pin(Current Monitoring) : Open?

 

I also received another question about reverse current protection.

Does this protection work at the condition that Vin is above 2.7V(VIn>=2.7V)? (When the Vin is below 2.7V, the reverse current protection doesn't work?)

Regards,

Yamaguchi

  • Hi Team,

    I received additional questions from the customer.

    Could you also tell me how to treat PGTH-pin when they don't use this pin?

    4. PGTH-pin : Open or  tied to ground?

    The customer now intends to treat each pin as follows.  Are these pin connection below ok?

    1. DMODE-pin(Diode Mode): Open

    2. PGOOD-pin(Power Good) : tied to ground

    3. IMON-pin(Current Monitoring) : OPEN?

    4. PGTH-pin :  tied to ground

    OVP :  tied to ground

    FLT : OPEN

    Regards,

    Yamaguchi

  • Hi Yamaguchi,

    DMODE, IMON and FLT pins can be left OPEN

    PGOOD, PGTH and OVP pins can be connected to GND

    Does this protection work at the condition that Vin is above 2.7V(VIn>=2.7V)? (When the Vin is below 2.7V, the reverse current protection doesn't work?)

    Yes, the back-to-back connected MOSFET configuration provides reverse current protection even for Vin <2.7V

    Best Regards, Rakesh