Tool/software: WEBENCH® Design Tools
I used WEbench to design +12vto -18volts supply.
I have many problems:
1-with a 009 rs resistor the maximum currentLM25088-2_12V_TO_-18V_2A.pdf is around 1.25 A instead of 2 , but with my personnel calculation a 0.011mohm should be ok.
if I disable de HICCUP mode, by shorting Cramp capacitor , i can reach mode dans 4 A , in fact de current limiter look disable ALSO.
2-But the big issue is the current sink from 12 volt start at 3.9 Amp for a -18volt output current of 2 ( 77% eff) AND reached over 7 Amp after many second
that look like a device going to latch up and short...
also in my design I add a big 150uf polymer, if i do not used it , I have a lot of noise at the output
in include my design, the only difference is I used a -2 device instead of -1 device.