Dear TI,
I have a battery with 5200mAh nominal capacity spec. I set the charger termination current to C/20 (260mA) and the battery capacity I get just around 5130mAh. Then I reduced the charger termination current to C/40 (130mA) and the battery capacity able to achieved >5200mAh. What are the side effects to the battery if I reduce the charger termination current?
Thank you.
Best regards,
Fariz