This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24196: Output voltage control for BQ24196

Part Number: BQ24196

I have a requirement in which input is 5V, 3A,  I need to have a LiIon battery backup.  My output should be 3.3V for both conditions: 1) When I have input 5V supply 2) When I am running on battery 

Can I use this part ?  If yes, please send relevant schematics and configuration parameters

Regards,