Other Parts Discussed in Thread: TPS1H100-Q1
Hi Team,
We are using TPS2HB16A to Protect the Load from the OverCurrent condition. The Current limit we set was 4.1A with 25K IRlim resistor and When we connect the load it won't turn on (Max load current was 1.5A). We think it is because of the Surge current which the device is taking at the time of boot up. When we used the resistive load then it works as expected. So to Slow the Trip Timing of IC we used a 0.47uF ceramic cap in parallel with the Current Limit resistor (IRlim) and it worked. so is it recommended to use the capacitor parallel to the Current Limit resistor? or is there any other solution to increase the trip detection time for the Current limit to allow the surge current to pass.
Thanks,
Nikhil