Hello,
I am designing a boost converter based on TPS61288:
- input voltage: [9V to 16V]
- output voltage: 16V
While reading the datasheet I found out that switching peak current limit is 15A.
I think I can't take this current data and say this component could give 8.4A @16V (9V*15A=135W). I didn't find any equation in the TPS61288 datasheet that could give an approximate value of maximum output current based on voltage and internal current data (or maximum power).
Thank you in advance for your support.
Best regards,
Samy