I have a problem with my Phase-Shifted Bridge going into Burst Mode. I have two phase-shifted bridges side by side on the same PCB and connected to the same high voltage bus with LC filters on the front-end of each bridge. The bridges are synchronized (both in slave mode) and outputting different voltages. The problem is that when one of the bridges goes into burst mode it induces a disturbance on the other bridges output (see screenshots). I'm not sure if it's the modulation on the high voltage bus that's causing the issue or if it's parasitics. I do know that the problem goes away when the controller exists burst mode.
I'm using the UCC28951 controller and have set Rtmin to 10k (the lowest value allowed by the datasheet). I'm trying to prevent the controller from going into burst mode, but previous forum posts show that there is no way to completely disable it. Can I set Rtmin to less than 10k? What are the implications of doing this? Is there any other way to prevent burst mode or mitigate its effects to the output voltage ripple?