Hi,
I use BQ25890 and use a 103AT NTC thermistor on the battery pack.
I find that, the TSPCT will becomes 0 when the SOC is about 2%, as shown below.
You can see that after the SOC drop to 2% for a while, the TempBatt jump to 84.8C. I looked at the TSPCT, it is 0 at that time.
At first, I think maybe the Voltage drops to Vsysmin(3.5V) and the BQ25890 turns into VSYSMIN mode, maybe at that mode, the TSPCT can not work normally.
But I find the VSYS_STAT is still 0, which means the BQ25890 is still at normal regulation mode.
So, what happens?
Thank you.
Frank