This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD9090A: Current Consumption during soft-off

Part Number: UCD9090A

Hi

We want to use the UCD9090A in a Battery powered application.
We want to use the PMBus_CNTRL pin to control the sequence-on / -off.
Thus we would like to know how much the current consumption of a UCD9090A is with sequence-off (PMBus_CNTRL = low)

In the Datasheet SLVSDD7A, 6.5 Electrical Characteristics
Iv33A = 8mA, Iv33dio = 2mA, Iv33D = 40mA
are given, with the note 1) "Typical supply current values are based on device programmed but not configured, and no peripherals connected to any pins."

So this seams to be the "active" state with no peripherals attached.
Is there also a measurement given, for PMBus_CNTRL low, in the same configuration (no peripherals attached) ?

Best Regards
Alex