Part Number: UCC28180
Hello,
My customer is using UCC28180 for 3KW PFC design. They are confront two problem regarding input current distortion.
Here is the schematic:
With two 0.01mohm in parallel, they found oscillation on the peak of input current and ICOMP output goes flat, as the following figure:
(Yellow: Input voltage, Green: Input AC current; Blue: ICOMP)
They had tried to decrease the current sense resistor to 3mohm, the current went away as the following figure.
(Yellow: Input voltage, Green: Input AC current; Pink: inductor current)
However, with the same condition just when ambient temperature exceeds 45C, one of the current peak goes abnormal. As follow figure.
(Yellow: Input voltage, Green: Input AC current; Pink: inductor current)
They have tried with compensation, but it seems not work.
Could you help analyze above two scenarios and suggest possible cause?
B.R
Paul