In some applications we have problems in charge mode, because the wire adds up to 1.5 volt to the cell voltage, even with a 2-3A only. It is not possible to make a better connection. The internal circuit of 1499q properly stops charging, but we would like extend the range. The component involved are R1,R3,R4,C3 (1402 board), Let's try to modify R3 to 1.5K (1k org) without modifications. Do you have you a suggestion or workaround?
Thanks and bst rgds
Massimo