This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25887: 2s charger with LED interface for capacity indicator

Part Number: BQ25887
Other Parts Discussed in Thread: BQ25883,

Hi team,

Customer is looking for 2s battery charger with LED interface for remaining capacity indicator, do we have any charger part with such kind of function?

Thanks and Best Regards,

Will 

  • Will,

    What will be your input voltage?

    What will be your charge voltage?

    What will be your charge current?

    Do you require cell balancing?

    Will this application be host controlled or standalone?

    Thanks,

    Ricardo

  • Ricardo,

    What will be your input voltage? 5V

    What will be your charge voltage? 8.4V

    What will be your charge current? 1~2A should be OK.

    Do you require cell balancing? Both would be OK.

    Will this application be host controlled or standalone? Both would be OK.

    Thanks and Best Regards,

    Will

  • Hi Will,

    You can consider BQ25883 or BQ25887 (with integrated cell balancing) for your application. Both these chargers have integrated ADC to monitor the battery voltage, which could help you roughly estimate capacity of battery based on battery voltage, but a fuel gauge is highly recommended to indicate the battery capacity (SOC and SOH) accurately taking in consideration dynamic load.