Other Parts Discussed in Thread: TPS56221
Dear Power Design Expert,
I have a design with TPS56121. the parameters are from Webench, it is a 12V input, 9V, 9A output.
it is used to drive a TEC, the R125 will be set to 2.8V or 0.48V to control the output voltage to 1.6v or 8.5V.
the board is 4 layers. one full ground layer. The board can output the correct voltage and current without a problem, but for some reason, it causes the system overall noise level to rise. after some measurement, I notice that the input cap has very high transaction noise as in the following waveform. I attached the waveform, schematic, and layout. for this kind of problem, is there a general rule to troubleshoot. for example, is the components value, placement, layout trace should be paid attention, how to design the next test to improve the design? where should I start to respin the board?
high current power regulator is not easy to design. hope I can get some suggestion, appreciate your help.