Other Parts Discussed in Thread: TPS62825, TPS62869
Hi team,
Does it support 3.1Vin to 3Vout with up to 2A current?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Jerry,
TPS62864 can support up to 1.675V.
If you are looking for this type of operation at 2A, you should probably look at TPS62825.
Or is there a specific reason why you picked TPS62864 here ? Is it related to I2C communication?
Let me know if you have any other questions!
Thanks,
Dorian
Hi Dorian,
I'm looking for a solution for 0.4V to 3V adjustable output. I just saw TPS6286x can support 0.4V.
Hello Jerry,
You can also have a look at the TPS62869 which offers different output voltage ranges with same package and BOM adressing from 0.2V up to 3.35V.
Let me know!
Regards,
Dorian