This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LMR33630: Simulate the negative output

Part Number: LMR33630


Tool/software: WEBENCH® Design Tools

Hi Team,

We would like to achieve below I/O by using LMR33630. (

1. Vin = 5V ; Vout = -10V ; Iout = 1.5A

2. Vin = 12V ; Vout = -10V ; Iout = 1.5A

Could you help provide simulation file which is using above I/O spec? (Like webench or simplis)

Regards,

Roy